You are here:Home1/Solutions2/Cable Logging Monitoring
Solution
Cable Logging Monitoring
In cable logging systems, the tension of the cables need to be monitored to maintain a safe working environment, and prevent any potential equipment damage. A system is needed to monitor the tension of the cables.
In cable logging systems, the tension of the cables need to be monitored to maintain a safe working environment, and prevent any potential equipment damage. A system is needed to monitor the tension of the cables.
Interface Solution
Interface’s WTSATL Lightweight Aluminum Wireless Tension Load Link is attached to the cables of the logging yarder, where tension forces are monitored. Force measurements are transmitted to the WTS-HK-S Next-Generation Wireless Handheld and to the customers computer or laptop through the WTS-BS-4 USB Industrial Base Station. With the WTS Log100 Software,the customer is able to graph and log the data results with this software onto their computer.
Results
The logging company was able to monitor the tension of their cables on the logging yarder during logging operations to ensure a safe working environment.
Materials
WTSATL Lightweight Aluminum Wireless Tension Link
WTS-HK-S Next-Generation Wireless Handheld
WTS-BS-4 USB Industrial Base Station
WTS Log100 Software (graphing and logging software, included with WTS-BS-4)
Customer PC or Laptop
How it Works
The WTSATL Lightweight Aluminum Wireless Tension Link is attached to the cable line on the yarder.
Tension results are measured and monitored using the WTS-HK-S Next-Generation Wireless Handheld.
The customer can also graphic and log the results with included Log100 software onto their computer.