Solution


Wave Energy Generator

A scientist has been tasked to create electricity by using the energy that is generated by ocean waves.


WaveGeneratorGraphic Color

Summary

  • Customer Need / Challenge

    A scientist has been tasked to create electricity by using the energy that is generated by ocean waves.

  • Interface Solution

    As electricity is generated by ocean waves, an Interface load cell will measure tether line tension using a submersible ITCA Tension and Compression Load Cell. The mooring line was attached to the load cell base and the platform generator was connected to the load cell hub. This measured the forces that were generated by the ocean waves and data was later analyzed by the customer’s Data Acquisition System (DAQ).

  • Results

    Scientists used force data to make adjustments to tether line. Also, if tether line breaks free, the scientist can be notified immediately to reattach the tether line.

Materials


  • ITCA Tension and Compression Load Cell

How it Works


  1. The ITCA Tension and Compression Load Cell is connected between a mooring line on the sea floor and a wave energy generator platform.
  2. The load cell cable is connected to customer’s DAQ.
  3. As electricity is generated by ocean waves, force readings from load cell are recorded in the DAQ.
  4. Results are analyzed by a scientist and adjustments to the tether line are made accordingly.

Download PDF