A car manufacturer wants to test the power steering for their vehicles. They want to test the linkage tension and compression between the rack and pinion.
A car manufacturer wants to test the power steering for their vehicles. They want to test the linkage tension and compression between the rack and pinion.
Interface Solution
On a test frame, Interface’s 1200 Standard Precision LowProfile™ Load Cell is installed at the end of the rack and pinion actuator. As the wheel is turned, the load cell tests the push and pull forces. Force measurements can be displayed in real time using the highly accurate 9870 High-Speed High Performance TEDS Ready Indicator.
Results
Interface’s 1200 Standard Precision LowProfile™ Load Cell successfully measured the tension and compression between the rack and pinion of the customer’s MDPS system.
Materials
1200 Standard Precision LowProfile™ Load Cell
9870 High-Speed High Performance TEDS Ready Indicator
Customer’s MDPS test frame
How it Works
The 1200 Standard Precision LowProfile™ Load Cell is installed at the end of the rack and pinion actuator.
As the wheel turns, the lateral push and pull forces are tested to determine the strength of the rack and pinion link.
Force measurements can be displayed in real time using the highly accurate 9870 High-Speed High Performance TEDS Ready Indicator.