Solution


Outdoor Festival Wind Monitoring

An outdoor festival is occurring in a large outdoor venue for multiple days. Outdoor stages pose a risk towards high wind speeds, which need to be monitored in case a storm passes through. This is to ensure safety for all personnel on site of the festival to avoid any accidents.


OutdoorFestivalWindMonitoring Color

Summary

  • Customer Need / Challenge

    An outdoor festival is occurring in a large outdoor venue for multiple days. Outdoor stages pose a risk towards high wind speeds, which need to be monitored in case a storm passes through. This is to ensure safety for all personnel on site of the festival to avoid any accidents.

  • Interface Solution

    Interface suggests installing the WTS-WSS Wireless Wind Speed Transmitter Module on the outdoor stage. Wind speed results are wirelessly transmitted to the customer’s PC through WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure. It can also be transmitted to the WTS-HK-S Next-Generation Wireless Handheld. Data can be displayed, logged, and graphed with supplied Log100 software.

  • Results

    Interface’s WTS-WSS Wireless Wind Speed Transmitter Module combined with Interface’s Wireless Telemetry System was perfect to monitor the wind speed during the outdoor festival.

Materials


  • WTS-WSS Wireless Wind Speed Transmitter Module
  • WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure with included Log100 Software
  • WTS-HK-S Next-Generation Wireless Handheld
  • Customer Laptop

How it Works


  1. The WTS-WSS Wireless Wind Speed Transmitter Module is installed to the outdoor festival stage.
  2.  The WTS-WSS captures the wind speeds wirelessly transmits it to the customer’s PC through the WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure. Customer’s also have the option of using the WTS-HK-S Next-Generation Wireless Handheld. Results are displayed, graphed, and recorded with supplied Log100 software.

Download PDF