The customer needs to measure pedal force in relation to the distance the pedal is pushed during automobile testing.
Interface Solution
As pedal is pushed, force is measured by BPL Pedal Load Cell and distance is measured by LVDT. Results are shown graphically and on a display while the data is being logged to a CSV file by model SI-USB4.
Results
Customer objective has been achieved. When pedal test was executed, the force measurement and distance measurement were simultaneously displayed, graphed and logged for examination in their lab.
Materials
BPL Brake Pedal Load Cell
LVDT sensor
SI-USB4 4-Channel USB Interface Module
Customer PC or laptop
How it Works
The BPL Brake Pedal Load Cell securely mounted on the top of the brake pedal, and the customer’s LDVT is installed on the back of the braking assembly.
The jet engine is ignited and produces a full thrust.
Both the BPL and LDVT is connected to the SI-USB4 4-Channel USB Interface Module. A brake test is performed and the force.
A brake test is performed and the force measurements are displayed, graphed, and logged onto the customer’s PC when connected to the USB connection of the SI-USB4.