Illustrated Application Note


Rescue Helicopter Hoist Test

A customer wants to test the strength of the cable line used in the hoist of their helicopter during rescue missions and situations.


RescueHelicopterGraphic Color

Summary

  • Customer Need / Challenge

    A customer wants to test the strength of the cable line used in the hoist of their helicopter during rescue missions and situations. They want to see if both the cable and the hoist can withstand a heavy load safely, and for long periods of time while the helicopter is in flight.

  • Interface Solution

    Interface’s WTSSHK-D Wireless Crosby™ Load Shackle is attached to each mooring cable in use. Results are sent to the customers through the WTS-BS-4 USB Industrial Base Station when connected to the customer’s supplied PC computer. Data can also be transmitted to the WTS-HK-S Next-Generation Wireless Handheld, giving the customer the option to view mooring cable line tension.

  • Results

    The customer was able to add a heavy load to the end of the helicopter hoist, to ensure it is strong and safe enough to carry both rescue personnel and objects while being in midair.

Materials


  • WTSSHK-D Wireless Crosby™ Load Shackle
  • WTS-HK-S Next-Generation Wireless Handheld
  • WTS-BS-4 Industrial USB Base Station
  • WTS Toolkit Software & Log100 Software Included
  • Customer PC or Laptop

How it Works


  1. The WTSSHK-D Wireless Crosby™ Load Shackle is installed at the end of the hoist.
  2. A heavy load is attached to the shackle at its maximum capacity, and tested through mid flight in order to monitor the condition of the helicopter hoist.
  3.  Data is transmitted wirelessly to the WTS-HK-S Next-Generation Wireless Handheld, and also to the customers PC for logging and graphing information.

Download PDF