Solution


Tablet Hardness Testing

A pharmaceutical tablet producer wanted to test and monitor the hardness of the tablets being created in their tablet forming machine.


TabletHardness Color

Summary

  • Customer Need / Challenge

    A pharmaceutical tablet producer wanted to test and monitor the hardness of the tablets being created in their tablet forming machine.

  • Interface Solution

    Interface’s SML Low Height S-Type Load Cell was mounted to the hardness device inside the tablet forming machine. The SML Low Height S-Type Load Cell was then connected to the 9870 High-Speed High Performance TEDS Ready Indicator to record the force measurements.

  • Results

    The tablet producer was able to verify and test the specific hardness needed for their tablets being produced by their tablet forming machine.

Materials


  • SML Low Height S-Type Load Cell
  • 9870 High-Speed High Performance TEDS Ready Indicator

How it Works


  1. The SML Low Height S-Type Load cell was customized to fit into the hardness testing device inside the tablet forming machine.
  2. The output of the SML was connected to the 9870 High-Speed High Performance TEDS Ready Indicator.
  3. The customer was able to calibrate and clarify the specified hardness for the tablets being formed.

Download PDF