Customer would like to crush test a specimen in their linear stand. The customer would like to use force to determine when the deformation actually occurs.
Customer would like to crush test a specimen in their linear stand. The customer would like to use force to determine when the deformation actually occurs.
Interface Solution
Interface provided Model 1210 Precision LowProfile® Load Cell with internal amplification of 0-10VDC Output.
Results
Amplified Model 1210 Precision LowProfile® Load Cell was installed into the load string of the customer’s load frame and the scaled analog output from the load cell was connected to the customer’s instrumentation. When the force levels reached the crushing point, the customer’s software was able to read the output of the amplified load cell and record the value.
Materials
1210 Precision LowProfile® Load Cell
Customer supplied linear test stand
How it Works
Amplified 1210 Precision LowProfile® Load Cell was installed into the load string of the customer’s load frame.
Scaled analog output from the load cell was connected to the customer’s instrumentation.
When the force levels reached the crushing point, the customer’s software was to read the output of the amplified load cell.