A tire production company wants to put their tires under a stress test. They want to research the dynamic control capabilities of their tires. They want to measure both the torque and lateral force of the tire.
Interface Solution
Interface suggests using the AT105 Contactless Force/Torque Transducer to measure the lateral force and torque of the tested tires. Torque and force results can be displayed and graphed when connected to theSI-USB4 4 Channel USB Interface Module.
Results
After conducting a stress test on their tires, the tire production company was able to record and log the measurements of the torque and lateral forces implemented on their tires.
Materials
AT105 Contactless Force/Torque Transducer
SI-USB4 4 Channel USB Interface Module with supplied software
Customer PC or Laptop
How it Works
The AT105 Contactless Force/Torque Transducer is installed in the customer’s tire friction test track.
The tire was tested on the company’s test track where torque and lateral force was measured..
The SI-USB4 4 Channel USB Interface Module was able to log and graph both the torque and force results from the tire stress test.