Customer is looking for a way to verify if the load cell is in “good working order” for an upcoming test.
Interface Solution
Interface proposed a solution with the customer’s supplied verification load frame, Model 1210 Precision LowProfile® Load Cell, connected with Model SI-USB4 4-Channel USB Interface Module.
Results
Customer installed their load cell and Model 1210 Precision LowProfile® Load cell into the verification load frame, and applied forces were displayed and recorded by Model SI-USB4 4-Channel USB Interface Module for review and record keeping on customer’s computer.
Materials
1210 Precision LowProfile® Load Cell
SI-USB4 4-Channel USB Interface Module with included setup, logging, and graphing software
Customer’s verification load frame
Customer’s test load cell
Customer’s supplied PC computer
How it Works
Customer installed their load cell to the customer’s verification load frame, connecting it to 1210 Precision LowProfile® Load Cell.
Customer applied the specific load by turning the manual actuator.
Applied forces were measured by the 1210 Precision LowProfile® Load Cell.
Results from the load cell under test and from the 1210 Precision LowProfile® Load cell were displayed and recorded by the SI-USB4 4-Channel USB Interface Module for review and record keeping on customer’s computer.