You are here:Home1/Solutions2/WTS Yacht Rigging Inspection
Solution
WTS Yacht Rigging Inspection
A customer wants to have a complete rigging inspection to make sure the mast, still lines, and all movable hoisting lines are functional and meet the proper specifications for sailing.
A customer wants to have a complete rigging inspection to make sure the mast, still lines, and all movable hoisting lines are functional and meet the proper specifications for sailing. The customer wants to test the tension of the forestay, shroud, and backstay cables. They also want to test the tension of the movable lines when sailing.
Interface Solution
With Interface, Inc’s WTSSHK-B Wireless Crosby™ Bow Load Shackle paired with the WTS-HK-S Next-Generation Wireless Handheld, the customer can switch and view between multiple shackles being tested. The WTS-BS-4 USB Industrial Base Station can also be attached to the customer’s PC to display realtime measurements from the shackles and log data.
Results
The customer was able to conduct both a running and standing rigging inspection of their ship or vessel, and was able to determine if all lines were functional and met safety standards.
Materials
WTSSHK-B Wireless Crosby™ Bow Load Shackles
WTS-BS-4 Industrial USB Base Station
WTS-HK-S Next-Generation Wireless Handheld
WTS Toolkit Software & Log100 Software Included
Customer PC or Laptop
How it Works
WTSSHK-B Wireless Crosby™ Bow Load Shackles are attached to the vessels forestay, shroud, and backstay cables.
The measurement at a is transmitted wirelessly to the WTS-HK-S Next-Generation Wireless Handheld, where the customer is able to view all results of all shackles in real-time.
The WTSSHK-B Wireless Crosby™ Bow Load Shackles also transmit information to the WTS-BS-4 USB Industrial Base Station, attached to the customer’s PC/Laptop for real-time results.