Interface Solutions Designed for Infrastructure Challenges
All infrastructure, big and small, needs to be designed with safety and durability in mind. Take for instance the massive amount of design, engineering and quality control that goes into a suspension bridge requires testing before and after it’s built. Not only does it need to be constructed with supreme accuracy, but it also needs to be tested and monitored constantly to ensure it’s safe for use, especially as often infrastructure projects are exposed to extreme elements.
Among the various tools and technologies used to build and test infrastructure designs, sensors play a substantial role. Interface has served infrastructure industry suppliers and customers since our founding more than 50 years ago. Force and torque measurement products including Interface load cells, torque transducers, load pins, load shackles, tension links and instrumentation are involved in a wide variety of infrastructure applications including construction and maintenance of bridges, roads, transportation systems, communication structures, water and electrical facilities, and numerous inventions that are used to build, test, support, maintain and monitor performance of these critical projects around the world.
Accuracy and reliability of Interface solutions are a key factor in measuring structures and components that are exposed to hazardous or weather-related conditions, heavy loads and constant use. Our precision load cells, rugged load pins, wireless and digital instrumentation, along with multi-axis sensors and robust torque transducers are a top choice for those engaged in infrastructure engineering projects and testing.
A few examples of how Interface products have been used on infrastructure applications over the years are noted below. The following examples are also found with many others here /solutions/infrastructure/.
Concrete Dam Flood Monitoring
A customer was looking for a solution to monitor a concrete dam and be notified when it reached high flooding levels. Interface provided WMC Miniature Sealed Stainless Steel Load Cells with multiple WTS-AM-1E Wireless Acquisition Modules connected to the load cells. This solution proved to be small enough and perfect for measuring compression and tension on the dam. The WMC Modules are installed on the arch of the dame and transmit data and notify the customer through Interface’s Wireless Telemetry System when flooding occurs. Check out the application here.
Hydropower Turbine Generator Monitoring
When a customer wants to monitor and detect turbine generator faults in their hydroelectric power plant located on a river, Interface can provide a T2 Ultra Precision Shaft Style Rotary Torque Transducer and attach it to the turbine generator with Interface’s Shaft Style Torque Transducer Couplings. When water from the river pushes through the penstock to the outflow, it moves the turbine blades, creating electricity through the generator shaft. Torsion measurements can be graphed and logged with the 9850 Torque Transducer and Load Cell Indicator catching any unusual fluctuations and vibrations. Using this solution, the customer can monitor, graph, and log the torque measurement results of the turbine generator. Learn more here.
Bridge Seismic Force Monitoring Solution
A customer wanted to monitor seismic activity that occurs to a bridge using force sensors to continuously monitor activity before, during and after earthquakes. They also wanted a wireless solution to avoid running long cables on the bridge. Interface provided an LP Load Pin custom made to fit the need. The load pin was used in conjunction with our WTS Wireless Telemetry System to monitor the force on the load without cables. Using this solution, the customer was able to monitor continuously, log results to the cloud and review the data. Read more here.
This is just a brief example of the applications throughout the infrastructure industry that Interface supports. A long list of additional applications that use Interface products includes:
Highways and Bridge Construction and Monitoring
Concrete Dam Measurement and Flood Monitoring
Transportation Heavy Equipment Testing
People Movers for Airports
Train Brakes Testing
Power Generation Equipment
Geotechnical Monitoring
Road Load Tests
Weight Bridges and Transportation Scales
Truck and Aircraft Weighing
Housing Mainframe and Skyscraper Construction Monitoring
Building Foundation Capacity Measurement
Bridge Seismic Force Monitoring
Cranes and Heavy Object Lifting
Structural Testing and Telecommunication Structures
Conveyor Belts
To learn more about Interface and our solutions for Infrastructure and other key industries, please visit our solutions page at staging.interfaceforce.com/solutions/.