Interface Helps Power the World
As technology and infrastructure have advanced to accommodate various forms of energy collection, the role of force measurement in the test and manufacturing of these machines has grown significantly. As a precision force measurement solutions provider, Interface has been a long-time partner to these global production and equipment customers in the energy industry. Interface sensors are used in different applications for various sectors, including oil, gas, wind, coal, solar, hydro, geothermal, nuclear, renewables and emerging alternatives around the world, as detailed in our energy solutions overview.
As a pioneer of load cell technology, Interface is recognized globally for providing the most accurate and reliable force measurement solutions utilized by energy market leaders and suppliers of parts, machines and technologies used in the sector. Accuracy matters for safety and reliability in energy-related test and measurement projects, engineering and product design, and in the original equipment manufacturing of components that require precision sensor technologies.
Interface products are used in several different applications for the energy marketplace. In fact, Interface is recognized as the prominent oil and gas solutions provider of force measurement solutions. These companies within the energy industry recognize Interface for product reliability, accuracy, and innovative design, as detailed here: Interface Most Promising Energy Tech Solution Provider.
To meet the growing demands for best-in-class energy market solutions, Interface recently launched our new downhole force measurement solution for high-pressure, high-temperature applications, the Interface Pressure Compensated Downhole Load Cell (IPCD). The IPCD is a Wheatstone bridge foil-gaged-based force measurement solution using proprietary compensation methods and designed to provide highly accurate force data in harsh environments, like those found in the oil and gas industry, while requiring limited maintenance compared to similar solutions on the market. Read the new IPCD technical white paper here.
Another area that is growing tremendously are alternative energy applications. Recently, Interface has been involved with projects involving wind and water energy, as well as playing a significant role in testing batteries on electric vehicles. Also, our energy customers come to us needing a custom force measurement solution to deal with these unique challenges for all energy types including thermal, radiant, chemical energy, nuclear, electrical, motion, sound, elastic, and gravitational energy.
Types of energy industry applications that utilize Interface products, services and technologies include:
- Oil and gas extraction equipment and parts
- Hydro power generation
- Windmill energy equipment
- Wireline spool tension control
- Fuel management and measurement
- Solar panel testing
- Hook load tension
- Torque tong monitoring
- Tool recovery and fishing
- Wave energy generator
- Downhole equipment
- Plug setting
- Calibration and equipment maintenance
- Storing crude oil and natural gas
- Transporting crude oil and natural gas
- Wireless monitoring equipment
- Activation of components and embedding sensors
We recently introduced a new solutions brochure on our energy solutions page. Additionally, we have included a few application examples below to give you an idea of the type of work we do and the customers we serve in energy:

Wave Energy Generator
A scientist had been tasked to create electricity by using the energy that is generated by ocean waves. As electricity is generated by ocean waves, an Interface load cell was used measure tether line tension using a submersible 3200 Hermetically Sealed LowProfile® Precision Stainless Load Cell. The mooring line was attached to the load cell base and the platform generator was connected to the load cell hub. This measured the forces that were generated by the ocean waves and data was later analyzed by the customer’s Data Acquisition System (DAQ). Scientists used force data to make adjustments to the tether line. Also, if tether line breaks free, the scientist can be notified immediately to reattach the tether line.
A customer wanted to improve the performance of a windmill by adjusting the blade pitch and measuring the torque generated as power ramps are studied. Interface offered a T2 Ultra Precision Shaft Style Rotary Torque Transducer which can be coupled between windmill blade propeller and electric generator. Information is sent to customer’s Data Acquisition System (DAQ). Using this solution, the customer was able to use torque data to determine the optimal blade pitch for the windmill and generate more power with less stress on the bearings.
Interface has worked with market leaders and innovators in the energy industry for decades. As new forms of energy are developed, new force innovations are required to confirm and test accuracy and reliability. As well as enhancements to machines, parts, equipment and materials, Interface is a supplier of choice for standard, modified and custom solutions. Our sensors are embedded into equipment, as well as part of everyday monitoring of force and pressure. To learn more about our work in the energy industry, visit our solutions page at https://staging.interfaceforce.com/solutions/energy/.
Additional Resources
Interface Leads Innovation in Oil and Gas Force Measurement
Announcing the Launch of the Interface Pressure Compensated Downhole Load Cell
Interface Pressure Compensated Downhole Load Cell White Paper