Load Washer Load Cells Versatility and Applications
Load washers are miniature force measurement sensors with a hollow, thru-hole center. Standard applications for these types of load cells include measuring tension, compression, and weight.
The primary advantage of this geometry is mechanical integration. The Interface Load Washer Load Cells design allows the sensor to become an integral part of an assembly, product, or system without requiring significant redesign of existing hardware. They are excellent for accommodating bolts, shafts, or cables.
Structurally, these sensors function as a stiff, cylindrical spring element instrumented with internal strain gages arranged in a Wheatstone bridge circuit. When an axial load is applied, the gages detect the minute deformation of the sensor body, converting mechanical stress into a proportional electrical signal. Characterized by high stiffness and minimal deflection, these sensors provide high-accuracy measurement in a compact footprint, specifically where space is constrained, and the force must be measured directly in the primary load path. Learn more in Load Washers 101.
Load Washer Applications in Varied Industries
The versatility of load washers makes them critical measurement devices across sectors such as manufacturing, maritime, energy, and healthcare. By integrating directly into machines, components, and test benches, these sensors provide high-precision force data in environments where traditional sensors are geometrically constrained.
Manufacturing
Load cells are needed during the manufacturing process for assembly verification. Attaching load cells to machines, as highlighted in this headset manufacturing equipment, ensures all parts of the headset, such as cables, microphones, and other components, are assembled correctly and securely. When production requires bolt applications, the best way to ensure the exact force is applied is to use load washers in a bolt fastening test.
Robotics and Industrial Automation
In robotic systems, load washers are integrated into joints and end-effectors to provide closed-loop force feedback. Mounting a load washer at a robotic gripper interface or within a swivel joint enables monitoring of assembly forces to prevent damage to fragile components. In broader industrial automation, they are essential for process control and safety monitoring. These sensors measure forces and torques during manufacturing, assembly, and chemical reaction mixing, including the axial thrust of mixing blades.
Medical Device Simulations and Testing
These sensors assess the performance and durability of prosthetic limbs, orthopedic implants, and surgical instruments. By integrating load washers into test fixtures, engineers can simulate the physiological forces implants experience over millions of cycles. They are also used in automated surgical systems to provide surgeons with data on tissue resistance during minimally invasive procedures.
Weighing Systems
In weighing applications, they are used on truck scales, tank weighing systems, and conveyor systems where the vessel or platform is secured via a central mounting bolt or post. The donut-style sensor makes it easier to integrate into existing apparatus and structures. In the entertainment industry, they are used to weigh large displays to ensure structural safety.
Energy and Power Generation
Load washers are common in renewable energy maintenance, particularly for monitoring the bolt tension that secures wind turbine blades to the hub. In nuclear and fossil fuel plants, additional applications include integrating load washers into pipe support systems and snubbers to monitor thermal expansion forces, ensuring that high-pressure piping does not overstress anchors as temperatures fluctuate. Electrolyzers convert electricity into hydrogen, and fuel cells convert the hydrogen back into electricity. Load washers monitor tie rods for these electrolyzers.
Heavy Equipment and Extraction
Load washers are integrated into cranes, hoists, and lifts to monitor lifting forces and prevent overloads. In the extraction industries, they are commonly used in drilling operations to monitor bit weight. Additional applications include measuring the clamping force on hydraulic tongs used to join drill pipes and integrating sensors into the pivot pins of booms and buckets on excavation equipment to track material volume and provide mechanical protection.
Maritime and Subsea
Specialized load washers are used in marine mooring systems and subsea deployments. They are placed in-line with underwater cables or winch systems to monitor tension during the deployment of Remotely Operated Vehicles (ROVs). By placing the sensor at the attachment point of a lifting eye, engineers capture dynamic loads from wave action and currents during subsea template installation.
Aerospace and Aviation
Load washers are used to test the structural integrity of aircraft components, including wings, fuselages, and landing gear. Beyond airframe validation, they provide precise measurements of axial forces in flight-control-surface linkage rods and landing-gear assemblies. Use in aircraft manufacturing equipment, including aircraft screwdriver fastening control applications, helps to control the precision needed in assembly. In space exploration, these sensors monitor preload in critical joints to prevent fatigue and verify the force required to actuate satellite deployment mechanisms. They are also integrated into flight simulators to provide accurate force feedback for pilot training.
Large-Scale Scientific Research
In particle accelerators and telescope installations, load washers provide precision for structural adjustments. They are common in the mounting assemblies of massive mirrors or magnets to ensure clamping forces do not distort sensitive components. This enables micron-level alignment required for high-energy physics and deep-space observations.

Automotive Engineering and Testing
Automotive applications include crash, durability, and component testing. Load washers measure the forces exerted on suspension, steering, and braking systems. During brake caliper testing, they are installed within the piston assembly to measure the clamping force on the rotor. In motorsports, these sensors are common in suspension linkages to measure cornering loads and downforce distribution. Additional use cases include real-time monitoring of pull-rod or push-rod assemblies to validate aerodynamic models against track data.
Interface Load Washer Load Cells

- LW General Purpose Load Washer Load Cell for measuring 5 to 40k lbf
- LWCF Clamping Force Load Cell for measuring 3.37k to 33.7k lbf
- LWHP14 Precision Load Washer Load Cell for measuring 11.2 to 22.5k lbf>
- LWMH1 Load Washer Load Cell With Mounting Holes for measuring 45 to 2.25k lbf
- LWMH2 Larger Load Washer Load Cell With Mounting Holes for measuring 112.4 to 4.5k lbf
- LWPF1 Press Force Load Washer Load Cell for measuring 450 to 22.5k lbf
- LWPF2 High-Capacity Press Force Load Washer Load Cell for measuring 22.5k to 135k lbf
- LWHP18 High-Capacity Precision Load Washer Load Cell for measuring 12k to 1,124k lbf
LWHP18 High Capacity Precision Load Washer Load Cell / #shorts
The versatility of the load washer stems from its ability to exist within the mechanical load path without necessitating substantial structural changes. Whether utilized for short-term validation in a laboratory or permanent installation, the load washer load cells provide critical data where conventional sensors are geometrically impractical.
By selecting the appropriate capacity and material specifications, engineers can implement load washers across nearly every industrial sector to improve safety, precision, and performance. Contact us to review your application requirements and determine which sensor might work best for you.